cancel
Showing results for 
Search instead for 
Did you mean: 

Point3D MCS

Genius
Genius

Hello,

 

I'm looking for a journal to do a Point3D from Machine coordinate system

thanks for your help

@mkn
3 REPLIES

Re: Point3D MCS

First thing to know is that there can be many MCS in a part, and you need to make one of them the active MCS. This requires being in the Manufacturing Applicaiton, and selecting or editing the mill_orient group, or one of the child operations.

This is what I would do interactively. You could do the same thing: 

  1. Check the preference to orient WCS to MCS (CsysOrientWcsToMcs)
  2. Set the preference True
  3. Select or Edit the MCS or operation (to make one MCS active)
  4. Define the point in WCS coordinates
  5. Restore the preference to its previous state.

 

 

Mark Rief
Retired Siemens

Re: Point3D MCS

Genius
Genius

it's a good idea ,but i must to edit a operation or MCS for changing the WCS , select is not enough.

I am going to try to think every time of putting my wcs on my MCS.

I thought that it was easier than that !! Smiley Frustrated

 

@mkn

Re: Point3D MCS

Genius
Genius

I finally found a solution.

From a character string, i create a 3D point which is related to my WCS

If anyone is interested, my code below.( i'm not a programmer ,there is certainly a more effective solution)

Thanks for this amazing website : http://www.nxjournaling.com/

Capture d’écran (6).png

 

 

 

 

 

 

 

Option Strict Off
Imports System
Imports NXOpen
Imports NXOpen.UF

Module GOTOPoint

Dim ufs As UFSession = UFSession.GetUFSession()

 Sub Main()
 
 
Dim theSession As Session = Session.GetSession()
Dim workPart As Part = theSession.Parts.Work
Dim lw As ListingWindow = theSession.ListingWindow

Dim goto_point As String  = InputBox("GOTO/:", "Coordonnées")
Dim words = goto_point.Split(","c)
Dim gotox = val(words(words.length - 3))
Dim gotoy = val(words(words.length - 2))
Dim gotoz = val(words(words.length - 1))
Dim lenght_goto As Integer = words.length

If goto_point = "" Then
MsgBox("GOTO Annulé!", MsgBoxStyle.Exclamation, "Erreur")
Exit Sub
End If

If lenght_goto > 3 Then
MsgBox("Trop de valeurs sur le GOTO", MsgBoxStyle.Exclamation, "Erreur")
Exit Sub
End If

       lw.Open()
REM Création Point3d Dim Pt As New Point3d Pt.X = gotox Pt.Y = gotoy Pt.Z = gotoz REM Création point -> WCS Dim ptObj As Point Dim originwcs As NXOpen.Point3d originwcs = WCS2Abs(Pt) ptObj = workPart.Points.CreatePoint(originwcs) ptObj.SetVisibility(SmartObject.VisibilityOption.Visible) lw.WriteLine("GOTO/" & goto_point) lw.WriteLine("X=" & gotox) lw.WriteLine("Y=" & gotoy) lw.WriteLine("Z=" & gotoz) lw.Close() End Sub Function WCS2Abs(ByVal inPt As Point3d) As Point3d Dim pt1(2), pt2(2) As Double pt1(0) = inPt.X pt1(1) = inPt.Y pt1(2) = inPt.Z ufs.Csys.MapPoint(UFConstants.UF_CSYS_ROOT_WCS_COORDS, pt1, _ UFConstants.UF_CSYS_ROOT_COORDS, pt2) WCS2Abs.X = pt2(0) WCS2Abs.Y = pt2(1) WCS2Abs.Z = pt2(2) End Function Public Function GetUnloadOption(ByVal dummy As String) As Integer 'Unloads the image when the NX session terminates GetUnloadOption = NXOpen.Session.LibraryUnloadOption.AtTermination End Function End Module 

 

 

@mkn