Cancel
Showing results for 
Search instead for 
Did you mean: 

Post Processor units

Experimenter
Experimenter

Hello Guys,

 

I've been working with one post processor in inches, works very well according to my requirements, but,  I need also the same post processor in millimeters, so I tried to generate a post using "Units Only Subpost" doing reference to my main post in inches, when I try to generate a program with the new post in millimeters the next messege appers:

 

Received an error 1740001

File name: D:\workdir\reference\NX1102_7\src\cams\no\ind\mom_post_parse.c, line number: 4009

Error Message: Can not find file

 

Do you know if this "Units Only Subpost" works? What I'm doing wrong to generate a sub post in different units?

 

Thank you, J.Cesar

1 REPLY 1

Re: Post Processor units

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you haven't already, this would best be posted in one of the NX Manufacturing forums (CAM or Postprocessing)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled