Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with KF's mqc_askDimensionText for angular dimensions

Experimenter
Experimenter

I'm cycling a file to get all the dimension values, NON inherited (non-kf) dimensions.

 

Using...

$dimensions << mqc_askDimensions(ALL);

 

loop
{
for $dim in $dimensions;
for $text is mqc_askDimensionText(first($dim));
do ug_printValues({nth(5,$text)});
};


Cycling the dimensions, any angular dimensions return back as whole values not decimal value.  All other dimension's values will return correct decimal values as displayed in the part.  Get same result if using mqc_askAnnotationText instead of mqc_askDimensionText.

Same results with angular PMIs.

 

Additional information:

If using mqc_askDimDecimalPlaces on an angular dimension, the correct decimal places value is returned, for example... 45.1234 will return 4 for decimal places but will return 45 as the value not 45.1234.

 

Any ideas or suggestions?

 

Thanks in advance.

2 REPLIES

Re: Problem with KF's mqc_askDimensionText for angular dimensions

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Sounds like a bug to me.

Did you search UGanswer?

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Problem with KF's mqc_askDimensionText for angular dimensions

Experimenter
Experimenter

Hello Ken

 

Yes I have searched for this in the UGanswer and did not found anything reported on this issue.

I will have to report this as an IR.

 

Thank you.