Cancel
Showing results for 
Search instead for 
Did you mean: 

Programatically query a part for a symbolic thread

Pioneer
Pioneer

I am in need of an custom application to programatically query a selected part to see if it contains a symbolic thread. If the part contains a symbolic thread, I would like to extract the "Callout" value for that specific thread. Any help would be greatly appreciated.

 

NX 9.0

VB.Net

4 REPLIES

Re: Programatically query a part for a symbolic thread

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Run the following code on a part that has a symbolic thread applied to a face.

 

Option Strict Off
Imports System
Imports NXOpen
Imports NXOpen.UF

Module Module3

    Dim theSession As Session = Session.GetSession()
    Dim theUfSession As UFSession = UFSession.GetUFSession()

    Dim lw As ListingWindow = theSession.ListingWindow

    Sub Main()

        If IsNothing(theSession.Parts.Work) Then
            'active part required
            Return
        End If

        Dim workPart As Part = theSession.Parts.Work
        lw.Open()

        Const undoMarkName As String = "report symbolic thread parameters"
        Dim markId1 As Session.UndoMarkId
        markId1 = theSession.SetUndoMark(Session.MarkVisibility.Visible, undoMarkName)


        For Each tempFeat As Features.Feature In workPart.Features
            If tempFeat.FeatureType <> "SYMBOLIC_THREAD" Then
                'skip to next feature
                Continue For
            End If

            lw.WriteLine(tempFeat.GetFeatureName)

            Dim myThreadParms As UFModl.SymbThreadData

            Try
                theUfSession.Modl.AskSymbThreadParms(tempFeat.Tag, myThreadParms)
                lw.WriteLine("callout: " & myThreadParms.callout)
                lw.WriteLine("form: " & myThreadParms.form)
                If myThreadParms.rotation = UFConstants.UF_MODL_RIGHT_HAND Then
                    lw.WriteLine("right hand thread")
                Else
                    lw.WriteLine("left hand thread")
                End If

            Catch ex As NXException
                theSession.UndoToMark(markId1, undoMarkName)
                MsgBox(ex.Message)

            Finally

            End Try

            lw.WriteLine("")

        Next


        lw.Close()

    End Sub

    Public Function GetUnloadOption(ByVal dummy As String) As Integer

        'Unloads the image when the NX session terminates
        GetUnloadOption = NXOpen.Session.LibraryUnloadOption.AtTermination

    End Function

End Module

 

Re: Programatically query a part for a symbolic thread

Pioneer
Pioneer

Hey Cowski, thanks for the reply and the code works great. I failed to mention one thing when making my original post. In order to select the correct symbolic feature (as there could be miltiplr symbolic features) I have changed the feature name to "Conn Thread" so in the part I am testing it on the part navigator shows "Symbolic Thread (65) "Conn Thread". I have looked through the object browser in Visual Studio for the options on UGModl.SymbThreadData and have not found anything to extract that portion of the feature. Any ideas on that one?

 

Thanks again,

Scott

Re: Programatically query a part for a symbolic thread

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In that case, you have supplied a custom name for the feature. You can look for it in the loop, something like:

 

        For Each tempFeat As Features.Feature In workPart.Features

            'look for named feature
            If tempFeat.Name <> "Conn Thread" Then
                'skip to next feature
                Continue For
            End If

            'make sure it is the right feature type
            If tempFeat.FeatureType <> "SYMBOLIC_THREAD" Then
                'skip to next feature
                Continue For
            End If

 

You won't find the custom feature name in the thread data, rather it can be found as part of the feature object itself (you can rename any feature type, not just thread features).

Highlighted

Re: Programatically query a part for a symbolic thread

Pioneer
Pioneer

Wow, that was too easy. Thanks again for the help it was exactly what I was looking for.

 

Regards,

Scott