Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Project point on to a curve with nearest distance

Valued Contributor
Valued Contributor

Hello

I have some how managed to project a point on a curve with nearest distance on to a curve

it takes huge efforts to achieve this thing in interactive NX session

can some one help to do it in easier way or get this functionality as a new enhancement in NX

 

Project_point_at_Nearest_Distance_on_Curve.jpg

CAD Methods Development NX11 and NX12
4 REPLIES 4

Re: Project point on to a curve with nearest distance

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Perhaps I'm missing something, but have you tried: menu -> analysis -> measure distance (type: distance, Distance: minimum, associative, create output geometry)? This will create a point on the composite curve and a line (which you can use as a vector) from the start point to the point on the line.

Re: Project point on to a curve with nearest distance

Valued Contributor
Valued Contributor

Hello,

works in NX11 and NX12 

any ways we are switching to NX11

doesnt matter if not working in NX9.0Smiley Happy

CAD Methods Development NX11 and NX12

Re: Project point on to a curve with nearest distance

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I saw NX 11 in your signature so I answered according to that version. I just now noticed the NX 9 in your screenshot. In NX 9, the measurement value will be accurate, but the created geometry won't be associative.

Re: Project point on to a curve with nearest distance

Valued Contributor
Valued Contributor
Thanks a lot for solution
CAD Methods Development NX11 and NX12