Cancel
Showing results for 
Search instead for 
Did you mean: 

Pulling help files directly from siemens.com

Gears Phenom Gears Phenom
Gears Phenom

Is it possible to have NX 11 go to https://docs.plm.automation.siemens.com/tdoc/nx/11/nx_help/ for all of the help files?

 

As an experiment, I set the following:

UGII_UGDOC_BASE_DIR=https://docs.plm.automation.siemens.com/tdoc/nx/11/nx_help
UGII_HTML_UGDOC=https://docs.plm.automation.siemens.com/tdoc/nx/11/nx_help/#uid:index
UGII_HELP_RELEASE_NOTES=https://docs.plm.automation.siemens.com/tdoc/nx/11/release_notes/
UGII_HELP_WHATS_NEW=https://docs.plm.automation.siemens.com/tdoc/nx/11/nx_help/#uid:index_whatsnew
UGII_CSHELP_DOCS=???
UGII_CSHELP_HTML_DOCS=???

Everything seems to work, except when you use F1 to get help on context.  Am I missing something, or is this as much as I can do?

 

Thanks,

 Dave

-Dave
NX 11 | Teamcenter 11 | Windows 8.1
5 REPLIES

Re: Pulling help files directly from siemens.com

Siemens Legend Siemens Legend
Siemens Legend

Hello Dave,

 

You have too much in your UGII_UGDOC_BASE_DIR. Try:

UGII_UGDOC_BASE_DIR=https://docs.plm.automation.siemens.com/tdoc

However, the easiest way to use is is to unset that variable (and possibly the others too). 

NX then automatically goes to the online documentation.

Regards,

Gerrit Koelewijn

Re: Pulling help files directly from siemens.com

Gears Phenom Gears Phenom
Gears Phenom

I have removed all of the ugii_ugdoc_ variables from the NX110env.dat file, uninstalled the documentation.  I checked the hard set env's, and nothing with docs.

 

Now I the help can't find the localhost:8282, and I'm not sure where that is being set, of if that is the default?

 

Looking in the NX log file, I see:

    UGII_UGDOC_BASE                  http://localhost:8282
    UGII_UGDOC_API_BASE              https://docs.plm.automation.siemens.com
    UGII_HELP_RELEASE_NOTES          http://localhost:8282/tdoc/nx/11/release_notes/#uid:index
    UGII_HELP_WHATS_NEW              http://localhost:8282/tdoc/nx/11/nx_help/#uid:index_whatsnew
    UGII_CSHELP_DOCS                 http://localhost:8282/tdoc/nx/11/nx_help
    UGII_CSHELP_API_DOCS             https://docs.plm.automation.siemens.com/tdoc/nx/11/nx_api
    UGII_CSHELP_DEFAULTS_DOCS        http://localhost:8282/data_services/resources/nx/11/nx_help/common/en_US/graphics/fileLibrary/nx/cust_defaults/nx11
-Dave
NX 11 | Teamcenter 11 | Windows 8.1

Re: Pulling help files directly from siemens.com

Phenom
Phenom

@DaveK wrote:

I have removed all of the ugii_ugdoc_ variables from the NX110env.dat file, uninstalled the documentation.  I checked the hard set env's, and nothing with docs.

 

Now I the help can't find the localhost:8282, and I'm not sure where that is being set, of if that is the default?

 

Looking in the NX log file, I see:

    UGII_UGDOC_BASE                  http://localhost:8282
    UGII_UGDOC_API_BASE              https://docs.plm.automation.siemens.com
    UGII_HELP_RELEASE_NOTES          http://localhost:8282/tdoc/nx/11/release_notes/#uid:index
    UGII_HELP_WHATS_NEW              http://localhost:8282/tdoc/nx/11/nx_help/#uid:index_whatsnew
    UGII_CSHELP_DOCS                 http://localhost:8282/tdoc/nx/11/nx_help
    UGII_CSHELP_API_DOCS             https://docs.plm.automation.siemens.com/tdoc/nx/11/nx_api
    UGII_CSHELP_DEFAULTS_DOCS        http://localhost:8282/data_services/resources/nx/11/nx_help/common/en_US/graphics/fileLibrary/nx/cust_defaults/nx11

For me works fine, maybe you have the variable in the environment PC variable.

Thank you...

Using NX 11 / RuleDesigner PDM

Re: Pulling help files directly from siemens.com

Siemens Legend Siemens Legend
Siemens Legend

Dave,

 

It seems you still have some variables set at the system level.

In my logfile it says:

    UGII_UGDOC_BASE                  https://docs.plm.automation.siemens.com
    UGII_UGDOC_API_BASE              https://docs.plm.automation.siemens.com
    UGII_HELP_RELEASE_NOTES          https://docs.plm.automation.siemens.com/tdoc/nx/11/release_notes/#uid:index
    UGII_HELP_WHATS_NEW              https://docs.plm.automation.siemens.com/tdoc/nx/11/nx_help/#uid:index_whatsnew
    UGII_CSHELP_DOCS                 https://docs.plm.automation.siemens.com/tdoc/nx/11/nx_help
    UGII_CSHELP_API_DOCS             https://docs.plm.automation.siemens.com/tdoc/nx/11/nx_api
    UGII_CSHELP_DEFAULTS_DOCS        https://docs.plm.automation.siemens.com/data_services/resources/nx/11/nx_help/common/en_US/graphics/fileLibrary/nx/cust_defaults/nx11
    UGII_CSHELP_FUSION_DOCS          https://docs.plm.automation.siemens.com/data_services/resources/nx/11/nx_api/common/en_US/graphics/fileLibrary/nx/fusion
    UGII_AD_CSHELP_DOCS              https://docs.plm.automation.siemens.com/tdoc/nx/11/ad_help

Please open a dos box and type : set UGII_UGDOC

and see what the result is.

 

Regards,

Gerrit Koelewijn

Re: Pulling help files directly from siemens.com

Gears Phenom Gears Phenom
Gears Phenom

Computer just needed a reboot, after all that, it's working now, thanks!!

-Dave
NX 11 | Teamcenter 11 | Windows 8.1