Cancel
Showing results for 
Search instead for 
Did you mean: 

Python code sample- Datum plane creation/resizing

Genius
Genius

If you need to generate or resize datum planes, here is some sample code that could help. The key was using 

datum_feat=datumPlaneBuilder.CommitFeature()
datum_feat.JournalIdentifier

 

def datum_plane(self, datum_origin, datum_normals, datum_corners):
        
        self.theLw.WriteLine('\n')
        self.theLw.WriteLine("Datum Plane function")

        
        for i in range(len(datum_corners)):
            datumPlaneBuilder = workPart.Features.CreateDatumPlaneBuilder(NXOpen.Features.Feature.Null)
            self.theLw.WriteLine('\n')
            self.theLw.WriteLine('\n')
            self.theLw.WriteLine('\n')

            #returns an NX.Open Plane object, from DatumPlaneBuilder class
            plane = datumPlaneBuilder.GetPlane()
            geom = []
            plane.SetGeometry(geom)
            plane.SetUpdateOption(NXOpen.SmartObject.UpdateOption.WithinModeling)

            #using dist from plane to origin and a surface normal to create the plane
            plane.SetMethod(NXOpen.PlaneTypes.MethodType.Coefficients)
            
            origin = NXOpen.Point3d(datum_origin[i][0], datum_origin[i][1], datum_origin[i][2])
            
            plane.Origin = origin

            #a, b, c coefficients
            normal = NXOpen.Vector3d(datum_normals[i][0], datum_normals[i][1], datum_normals[i][2])
            plane.Normal = normal
            plane.Evaluate()

            datumPlaneBuilder.ResizeDuringUpdate=False
            
            datum_feat=datumPlaneBuilder.CommitFeature()
            
            #need to get journal Identifier of datum plane and pass it as an object
            self.theLw.WriteLine("Datum feature is "+str(datum_feat.JournalIdentifier))
            
            #create instance of resize plane
            resizePlaneBuilder = workPart.Features.CreateResizePlaneBuilder(NXOpen.Features.Feature.Null)   
            datum_object = workPart.Datums.FindObject(str(datum_feat.JournalIdentifier))
            resizePlaneBuilder.Plane.Value = datum_object

            resizePlaneBuilder.ResizeDuringUpdate = False
    
            corner_pts = [None] * 4 
            
            #multiplying by a scale factor just moves the planes further out
            # to adjust size, recalculate your corner points
            corner_pts[0] = NXOpen.Point3d(datum_corners[i][0][0],datum_corners[i][0][1],datum_corners[i][0][2])
            corner_pts[1] = NXOpen.Point3d(datum_corners[i][1][0],datum_corners[i][1][1],datum_corners[i][1][2])
            corner_pts[2] = NXOpen.Point3d(datum_corners[i][3][0],datum_corners[i][3][1],datum_corners[i][3][2])
            corner_pts[3] = NXOpen.Point3d(datum_corners[i][2][0],datum_corners[i][2][1],datum_corners[i][2][2])
            resizePlaneBuilder.SetCornerPoints(corner_pts)
    
            resizePlaneBuilder.Commit()
            resizePlaneBuilder.Destroy()

            datumPlaneBuilder.Destroy()