Cancel
Showing results for 
Search instead for 
Did you mean: 

ReadMe.txt

Innovator
Innovator

When you make a new project it comes with the ReadMe.txt file. Which contains stuff like

User Exit Environment Variable Entry Point

Open Part USER_RETRIEVE ufget

New Part USER_CREATE ufcre

Save Part USER_FILE ufput

I was wondering are these used in the command prompt window? 

How do you use these?

1 REPLY

Re: ReadMe.txt

Siemens Phenom Siemens Phenom
Siemens Phenom

 

The way that these are used:  You set an environment variable using the string in all caps, to point to a custom .dll.  For example, you could define:

 

set USER_CREATE=C:\path\to\my\myNewPartProgram.dll

 

Then when NX starts, it takes note of that environment variable, and when you select File -> New, NX will try to load and run your .dll.

 

You can read about these in the NXOpen documentation for a more detailed description.