Cancel
Showing results for 
Search instead for 
Did you mean: 

Regarding error

Hello,
I am trying to compile my program but it displays message of NXException was caught and shows NX error status: 1.
Can any one tell me what kind of error is these.How should i overcome through these error.
2 REPLIES

Re: Regarding error

Siemens Phenom Siemens Phenom
Siemens Phenom

We'll need more information in order to help you.  You are seeing this error at runtime, not when you compile, correct?

 

Can you tell how far your program gets before the error occurs?

 

What is on the line of code that returns the error?

 

Have you digitally signed the program?

 

What language are you using?

 

If it is one of the languages that can be run as a Journal, does it work that way?

 

Re: Regarding error

Thanks for the reply.
The error occurred at the time of importing the template and the error also occur at the time of commit.