Cancel
Showing results for 
Search instead for 
Did you mean: 

Relationship notes in 2D not getting updated when the 3D attribute is changed

Valued Contributor
Valued Contributor

Hello All,

 

I have created some relationship notes in 2D which links to the 3D attributes. The issue that I am facing is the 2D notes are not getting updated with the new attribute value automatically whenever the 3D attribute value is changed. I was expecting an automatic update on the 2D notes since the text is linked to the attribute in 3D.

 

Is there something that I need to do after changing the 3D attribute value to update all the relationship notes in the 2D?

 

Thanks,

Shanmugam.K

 

 

2 REPLIES 2

Re: Relationship notes in 2D not getting updated when the 3D attribute is changed

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Shanmugam18 ,

 

Are you updating them programatically? If no, please provide the part, add a NX version tag in a post.

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: Relationship notes in 2D not getting updated when the 3D attribute is changed

Valued Contributor
Valued Contributor

@SamadhanGaikwad I am updating the attribute manually as well as programmatically. When doing using a program, I am creating the relationship attribute using code and I see no problem in that.

For manual updates, I do not see the attribute value getting updated in 2D.