Cancel
Showing results for 
Search instead for 
Did you mean: 

Release an *.exe from NX 11, VB.NET

Valued Contributor
Valued Contributor

I develop an .exe application with VB. NET run with NX (by Control + U), I add a button "Exit" so when I press this "Exit", my application can be released from NX. However,

if I use  

Me.Dispose()

 --> My application is still being held by NX 

 

If I use

Application.Exit

--> The NX will close 

 

Any suggestion to resolve the problem will be appreciated.

 

2 REPLIES

Re: Release an *.exe from NX 11, VB.NET

Siemens Phenom Siemens Phenom
Siemens Phenom

Try adding this to your module or class:

 


    Public Function GetUnloadOption(ByVal dummy As String) As Integer
        Return Session.LibraryUnloadOption.Immediately
    End Function

 

Note that you do not need to call it; if it is there, NX should know what to do with it.  This is commonly used in NX Open .DLLs to make them unload as soon as the program is finished.  I don't really run .EXE files from inside NX, so I am not sure I have ever tested this in an .EXE, but it should be a simple test.

 

If that does not work, then you might try creating a .DLL instead of an .EXE.

Re: Release an *.exe from NX 11, VB.NET

Valued Contributor
Valued Contributor

Now I got it, I would need to build .dll instead of *.exe.  I actually I got this function included in my *.exe.

 

Thanks for the help.