Cancel
Showing results for 
Search instead for 
Did you mean: 

Reprogram the Reset button available in Nx9 block UI styler

Pioneer
Pioneer

Hi

I want ro reprogram the Reset button available at right top corner so that if I click that botton it should prompt me before resetting the values. So is this possible to do in NX9. If yes please let me know how to do it.

 

Thanks

 

 

1 REPLY

Re: Reprogram the Reset button available in Nx9 block UI styler

Siemens Phenom Siemens Phenom
Siemens Phenom

 

We don't have a dedicated callback for the reset button, but the initialize_cb() is called when you press the reset button.

 

But be careful - it is ALSO called at other times, such as when the dialog is initially being presented, and when Apply or OK is pressed.  So if you try to interrupt it, it will interrupt it at all of those times, not just when you actually press reset.