Cancel
Showing results for 
Search instead for 
Did you mean: 

Revolved spline says its surface type is a torus

Creator
Creator

See attached file.  The two planar faces work fine.  But UF_MODL_ask_face_type (same with UF_MODL_ask_face_data) returns "toroidal" for the type of the revolved spline face.  Is this expected behavior?

 

For what it's worth, it appears that coercing the toroidal face to a spline using UF_MODL_extract_face seems to give a correct B-surface.  This is expensive, so I do not want to do it for all surfaces that claim to be toroidal.  How do I know which cases are the bad ones?

5 REPLIES

Re: Revolved spline says its surface type is a torus

Siemens Phenom Siemens Phenom
Siemens Phenom

In this case, NX did not make the surface toroidal (though it will, if it can).

 

The interactive Info-->Object function correctly identifies the surface type as "Revolved".

 

I think there's something wrong with the UF_MODL_Ask_Face functions, or the set of constants used as type codes. I don't know exactly what the problem is, but I found some old code of mine that contained a bizarre workaround. In that code, when I encounter a surface that is claimed to be toroidal, I read the minor radius. If that minor radius is zero, then I conclude that the "toroidal" claim is a lie, and the surface is actually of type "Revolved".

 

I realize that this is a pretty vague answer, but maybe it points you in the right direction.

 

If you can isolate the problem, please send in a PR.

 

 

山田
yamada

Re: Revolved spline says its surface type is a torus

Siemens Phenom Siemens Phenom
Siemens Phenom

SNAP gets the right answers, and SNAP is just calling NX/Open functions, so there must be a way. Using this code:

public class NXJournal
{
   public static void Main()
   {
      foreach(var body in Snap.Globals.WorkPart.Bodies)
      {
         foreach(var face in body.Faces) 
            Snap.InfoWindow.WriteLine(face.ObjectSubType.ToString());
      }
   }
}

I got the following results for your model: 

FacePlane
FaceRevolved
FacePlane

 Here is what I did in some old code:

myType = myFace.SolidFaceType;

if (myType == NXOpen.Face.FaceType.SurfaceOfRevolution)
{
   double minorRadius = GetSurfaceRadii(myFace)[1];
   if (minorRadius != 0)  myType = NX.ObjectTypes.SubType.FaceTorus;
   else myType = NX.ObjectTypes.SubType.FaceRevolved;
}

 

山田
yamada

Re: Revolved spline says its surface type is a torus

Legend
Legend

It may be off interest why NX still call the face toriodal.  The image below shows the poles for the revolved face.  Note that it is treating as having a major radius and two minor radii instead of the traditional major and single minor radius.

 

Image1.jpg

 

 

 

 

 

 

 

 

 

 

Frank Swinkels

Re: Revolved spline says its surface type is a torus

Legend
Legend

I should mention that Nx can treat this like a toriod only because the spline has the correct number of poles (4 poles which is what is used for a standard torus.  I am not saying that we have two radii.

 

Frank Swinkels

Re: Revolved spline says its surface type is a torus

Siemens Phenom Siemens Phenom
Siemens Phenom

This seems to work:

public class NXJournal
{
   public static void Main()
   {
      var workPart = NXOpen.Session.GetSession().Parts.Work;

      foreach(NXOpen.Body body in workPart.Bodies)
      {
         foreach(NXOpen.Face face in body.GetFaces()) 
            Snap.InfoWindow.WriteLine(face.SolidFaceType.ToString());
      }
   }
}
山田
yamada