Cancel
Showing results for 
Search instead for 
Did you mean: 

Rotating an object

Creator
Creator

Hello,

 

I am using UF_MODL_move_feature to rotate 2 objects in the same orientation. Is it better to use move from AXIS to AXIS or move from CSYS to CSYS?

Also, which object features shall I put in the move_data function?

 

Thank you

4 REPLIES

Re: Rotating an object

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

What type of objects are you trying to move?

I'd suggest using the Features.MoveObjectBuilder if possible. It will probably be easier to code for if it works for your situation.

Re: Rotating an object

Creator
Creator

I can not find the MoveObjectBuilder in Open C Reference Guide. Is there any other function that I could use?

 

Thank you

Re: Rotating an object

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Re: Rotating an object

Creator
Creator

Unfortunately, I can only use C...