Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Run a journal from a NXOpen tool

Experimenter
Experimenter

Hello all,

 

I want to play a journal file ( journal.vb)  from an NXOpen.Net (c#) program.

Since the run_journal.exe is working in batch I can't use it.

The journal.vb is created on the fly by an external tool and should be started by the startup dll.

 

Thank you in advance

3 REPLIES

Re: Run a journal from a NXOpen tool

Siemens Phenom Siemens Phenom
Siemens Phenom

Essentially, you're asking whether a program written in C# can call a program written in VB. The answer is yes, and a Google search will give you lots of info on the subject.

 

But, life is much easier if the two programs that need to communicate are written in the same language. So, why not record the journal in C#, or why not write the calling program in VB ??

山田
yamada

Re: Run a journal from a NXOpen tool

Experimenter
Experimenter

Hi Yamada,

Thank you for your reply. But it doesn't work as described. I cannot build the dll which is calling the journal file and don't know how to proceed.

RunJournal.JPG

 

Regards

Wolfgang

Re: Run a journal from a NXOpen tool

Experimenter
Experimenter
Ok, so it's working : Play = theSession.JournalManager.PlayDotNetJournal(@"C:\temp\Journal.vb",sargs);