Cancel
Showing results for 
Search instead for 
Did you mean: 

SET UGII_ROOT_DIR

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Hi

 

I am using NX 10.0.3 .  Now I set varible UGII_ROOT_DIR in system variable. When I open NX and see log file  UGII_ROOT_DIR is set to C....NX\UGII..  .How to set  UGII_ROOT_DIR ? 

 

thank you

2 REPLIES

Re: SET UGII_ROOT_DIR

Phenom
Phenom

I defined new system variables: Systems/Advanced System Settings

 

but there is a (full) explanation in the doc too

https://docs.plm.automation.siemens.com/tdoc/nx/10/nx_api/#uid:genid_environment_variables_36_1466

Production: NX9.0.3.4, NX10.0.2.6
Development: VB.NET (amateur level !)

Re: SET UGII_ROOT_DIR

Esteemed Contributor
Esteemed Contributor

Note he is asking about UGII_ROOT_DIR (not one of the custoimization ENVs)

 

Do you also have a "user" level system variable? (Top half of the "Environment variables" dialog)?

 

If you have both "system" (bottom half) and user (top half), the user over-rides the system

try opening a command prompt window and typing "Set UG" and see what it returns

 

How (exactly) are you starting NX?

Start -> All Programs --> Siemens... -> NX 10.0?

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled