cancel
Showing results for 
Search instead for 
Did you mean: 

STEP export NX parts with additional attributes

Experimenter
Experimenter

I could use some help..

 

I would like to Export an NX (7.5) assembly as STEP file with additional attributes.

Of course the export itself is not the problem, but exporting attributes is actually a problem.

 

- All STEP parts should have a named attribute with the value of purely the ItemID from Teamcenter, not a single character different.

 

In addition I have already programmed a journal for the STEP export and it works fine, but at this point it does not export (user) attributes. The descriptive part names automaticly receives "_A" when I open the STEP file; not suitable for what I need. 

 

Please help with the problem stated above, thanks in forward.