Cancel
Showing results for 
Search instead for 
Did you mean: 

Save As fails

Genius
Genius

hello,


when performing a SaveAs in VB .NET, if the save operation fails, NX remains in an inconsistent state
where the work part is the failed (non-existent) part, instead of rolling back to the old (good) part.

This is unfortunate and shouldn't happen.

Is there any way to rollback other then manually reopening the old part ?


Code example follows.
Running NX 7.5.


Tnx



             Dim partSaveStatus2 As PartSaveStatus
            Try
                partSaveStatus2 = Parts.Work.SaveAs(new_workPart)
            Catch ex As NXException
                MsgBox("part :  " & new_workPart & "   has failed :" & vbCrLf & vbCrLf & ex.Message & vbCrLf, MsgBoxStyle.Exclamation, "error" )
                Return
            End Try

 

6 REPLIES

Re: Save As fails

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You could add code in the Catch block to reset the work part...

Re: Save As fails

Genius
Genius

this is what I meant by "manually reopening the old part".

 

My point is :

 

1)  this situation should never happen in the first place

2)  is there any option to rollback without reopening the old part ?

 

 

 

 

Re: Save As fails

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Create an undo mark, if the save-as operation errors, roll back to the undo mark. If a new file was created during the save-as, you might want to close & delete it.

Re: Save As fails

Genius
Genius

I tried undo marks but they are only good to undo feature operations, they seem not to

be working for other commands.

Closing and deleting is just what I wished to avoid. I will issue a message error for

the user to have him to close the part.

Again, NX should prevent this inconsistent situation to happen in the first place :-/

I reported an IR for this and a PR 8254155 is going to be opened.

 

 

Re: Save As fails

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

When you start writing code, you are essentially saying: "Move over NX, I'll take care of this...". As such, it is your responsibility to handle any errors or other odd behavior that occurs. You have the tools to do what you need to do.

 

There are many things that can go wrong when writing files, many of which have nothing to do specifically with NX. At a bare minimum you should check that the target location exists and you have write permission. After the SaveAs operation, check the PartSaveStatus and take action accordingly.

Re: Save As fails

Genius
Genius

the "bare minimum" is what I expect NX takes care of.  What I'm expected

to do is to take care of my own business, not NX's.

In this case NX is assigning the work part to a file which is not there, something

not very smart and something I have no control over.

The "bare minimum" in this case means that NX should save FIRST and THEN, IF

the save is successful, assign the work part. It doesn't seem very difficult to me, in

fact it's just matter of fixing a bug.