Cancel
Showing results for 
Search instead for 
Did you mean: 

Save objects into a separate file

Creator
Creator

Hello everyone!

 

Is there a way to save the selected faces/objects in a separate model file? Let's say I've selected some faces using the Face Collector of the Block UI Styler and want to save them as a separate file in the backgroud. Or the same operation, but using the Select Object and selecting the bodies. What would be the way to go?

 

Thanks in advance!

1 REPLY

Re: Save objects into a separate file

Stefan_Pendl 3rd Gear
3rd Gear

You would have to extract the face geometry into face bodies.

Faces are part of bodies and can't be exported to a different part file.

 

I would do the task interactively and create the code based on the interactive workflow.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk Testing: NX12.0 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink

How to Get the Most from Your Signature in the Community