Cancel
Showing results for 
Search instead for 
Did you mean: 

Seeing NX9 Part Properties in Windows Explorer Column

frank_nx 1st Gear
1st Gear

I'm working in NX9 native.

Is there a tool that allows me to see custom part properties of an NX prt file in Windows Explorer? (Win7 64bit)

2014-11-19_54.gif

 

Thanks,

Frank Huysmans

Huysmans Metalen n.v.
2x NX 11.0.2.7 Mach Designer
on Win7 64bit
NX Beta Tester with focus on Sheet Metal
Command Finder is your friend
3 REPLIES

Re: Seeing NX9 Part Properties in Windows Explorer Column

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

If you have NX5 installed it is possible.

There was a dll that could do it:

select start > run and type regsvr32 "%ugii_base_dir%"\ugii\ugpropext.dll

 

You can then see the attributes in a Windows Explorer properties dialog (see image).

 

It was removed however from NX6 upwards. Why I'm not certain, but it must have been causing issues

so use the above information at your own risk.

 

2014-11-20_9-10-44.jpg

Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2

Re: Seeing NX9 Part Properties in Windows Explorer Column

Siemens Phenom Siemens Phenom
Siemens Phenom

Occasionally, in idle moments, I have considered the idea of exporting NX part file properties and writing then as "real" Windows properties. Then they'd be visible in Windows Explorer. You'd have to run this code on every "save", I suppose, to ensure that the Windows properties are kept up to date. Has anyone tried this?

山田
yamada

Re: Seeing NX9 Part Properties in Windows Explorer Column

frank_nx 1st Gear
1st Gear

When is your next "idle" moment? Smiley Wink

I would love to have a journal/macro that does that.

And I can imagine I won't be the only one.

Huysmans Metalen n.v.
2x NX 11.0.2.7 Mach Designer
on Win7 64bit
NX Beta Tester with focus on Sheet Metal
Command Finder is your friend