Cancel
Showing results for 
Search instead for 
Did you mean: 

Select Objects in Blockstyler

Pioneer
Pioneer
Hi, I am using Select Objects in Blockstyler. If i select PointOverlay property to true i can select any point (startpoint, endpoint etc) in drawing plus i get Point Dialog also. but when i set PointOverlay to false Point Dialog is gone, but at the same time i am not able to select points. I am placing the custom symbols with leader but i am looking for some functionality same as default ballon tool. I tried to set Selection::MaskTriple MT9( UF_point_type, 0, 0 ); duting intialize but it doesnt work when i set PointOverlap to false. TAK
1 REPLY

Re: Select Objects in Blockstyler

Phenom
Phenom

Look at the sample code on solution center.  Look for 'nx_api4845'

Suresh