Cancel
Showing results for 
Search instead for 
Did you mean: 

Select all and Escape Key

Phenom
Phenom

Hi,

via API there is a code that simulate the CTRL+A (select all) and the escape key (Esc) ?

Thank you...

Using NX 11 / RuleDesigner PDM

1 REPLY

Re: Select all and Escape Key

Gears Phenom Gears Phenom
Gears Phenom

A recording of a test journal with a CTRL+A selection returns

' Refer to the sample NXOpen application, Selection for "Select All" alternatives.

 

so it seems that the shortcut may not exist as part of a journal

 

The followig example in \X 9.0\UGOPEN\SampleNXOpenApplications\.NET\Selection will give (and I quote): alternatives to the code recorded while performing a ''Select All' using various filtering methods before an operation

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)