Cancel
Showing results for 
Search instead for 
Did you mean: 

Selection mask polygon geometry

Legend
Legend

Hello,

 

I'm having trouble setting my selectio mask for polygon geometry. I have read the post

http://community.plm.automation.siemens.com/t5/NX-Programming-Customization/Block-UI-Styler-How-to-s...

 

But I still don't manage to make it working. This is what I think my selection mask should be for a polygon body:

        Dim SelectionMaskPolygonBody(0) As Selection.MaskTriple
        
        With SelectionMaskPolygonBody(0)
            .Type = UF.UFConstants.UF_sfem_mesh_geometry_type
            .Subtype = UF.UFConstants.UF_sfem_mesh_geometry_body_subtype
        End With

        PolygonBodySelection0.SetSelectionFilter(Selection.SelectionAction.ClearAndEnableSpecific, SelectionMaskPolygonBody)

But I don't get any selection options when I run.

 

Kind regards,

Frederik

14 REPLIES 14

Re: Selection mask polygon geometry

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Re: Selection mask polygon geometry

Legend
Legend

Hello Cowski1,

 

I have read this post, but I can not figure out. From this post I expect that when I use: 

.type = UF_sfem_mesh_geometry_type
.subtype = UF_smesh_geometry_body_subtype 

 I should be able to select polygon bodies only. However, when I run the program I cannot select anything.

 

I did manage for another input, to set my mask for mesh.

 

Regards,

frederik

Re: Selection mask polygon geometry

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

These only allow selecting of FEM meshes, for regular faceted bodies you would need a different selection mask.

From %UGII_BASE_DIR%\UGOPEN\uf_object_types.h:

#define UF_faceted_model_type                   139
#define    UF_faceted_model_normal_subtype             0
#define    UF_faceted_model_cloud_subtype              1
#define    UF_faceted_model_promoted_subtype           2
#define    UF_faceted_model_jt_body_subtype            3
#define    UF_faceted_model_face_subtype               4
#define    UF_faceted_model_edge_subtype               5
#define    UF_faceted_model_map_subtype                6
Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Selection mask polygon geometry

Legend
Legend

Hello Stefan,

 

Using the UF_Faceted_model_type I get facet body as my mask.

 

But what I actually need is polygon body and polygon face. Do you kno w

 

regards,

frederik

Re: Selection mask polygon geometry

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What kind of polygon, where did it come from?

What application are you working in, modeling, manufacturing or FEM?

Have you checked the file I mentioned for a type that has polygon in its name?

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide
Highlighted

Re: Selection mask polygon geometry

Legend
Legend

Hello Stefan,

 

I'm working in the advanced simulation (FEM).

I want to have the mask set to polygon body and polygon face.

I have checked the file uf_obj_types.h for polygon, but it is not present.

 

In the link to the post from JimB you sent earlier, it is mentioned that polygon geometry is from the "UF_sfem_mesh_geometry_type" which I tried but doesn't work.

 

Regards,

Frederik

Re: Selection mask polygon geometry

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I would use the (legacy) UF_OBJ_ask_type_and_subtype call (or the new equivalent) to get the object's type & subtype as numbers.

Then look in the various "*types.h" files to find a "name" associated.

Note that not all types are in uf_obj_types.h - IIRC, some have been split off to other files.

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Selection mask polygon geometry

Legend
Legend

Thanks Ken_A,

 

This is a good pointer, but how do I call the UF_OBJ_ask_type_and_subtype?

 

According to the manual there is an NXopen.uf.ufobj.AskTypeAndSubtype, which acts as a wrapper for UF_OBJ_ask_type_and_subtype, but I cannot access this method.

 

This is the code I have:

Option Strict Off
Imports System
Imports NXOpen

Imports NXOpen.Utilities


Module Module2

    Sub Main()
        Dim theSession As Session = Session.GetSession()
        Dim theLW As ListingWindow = theSession.ListingWindow
        theLW.Open()

        Dim BasePart As BasePart = theSession.Parts.BaseWork
        Dim BaseFemPart As CAE.FemPart = CType(theSession.Parts.BaseWork, CAE.FemPart)
        Dim cAEBody1 As NXOpen.CAE.CAEBody = CType(BaseFemPart.FindObject("CAE_Body(1)"), NXOpen.CAE.CAEBody)

        Dim test1 As Int32 = Nothing
        Dim test2 As Int32 = Nothing

        UF.UFObj.AskTypeAndSubtype(cAEBody1, test1, test2)

        theLW.WriteFullline(test1.ToString)

    End Sub

End Module

 I get the error message:

"reference to a non-shared member requires an object reference"

 

Regards,

Frederik

 

 

Re: Selection mask polygon geometry

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

UF wrapper functions need an old tag, so you need to use the following.

In addition you need the UF session too.

 

UFSession.GetUFSession().UFObj.AskTypeAndSubtype(cAEBody1.Tag, test1, test2)

 

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide