Cancel
Showing results for 
Search instead for 
Did you mean: 

SelectionManager

Innovator
Innovator

How does the selection Manager work?

UI.SelectionManager.

 

What does the Selection.MaskTriple Do?

Any help would be helpful.

Thank you.

2 REPLIES

Re: SelectionManager

Siemens Phenom Siemens Phenom
Siemens Phenom

 

Good morning.  The selection mask triples allow you to specify what types and subtypes of objects can be selected.

 

In the Solution Center, search for:

 

nxopen  sample  selectionmanager

 

Then when the initial list of hits is returned, on the left side of the page, under Document Type, click on "nx_api".  This will show you 20 small examples that use the SelectionManager.

 

Re: SelectionManager

Honored Contributor
Honored Contributor

"Types" and "subtypes" help to categorize NX objects. Every NX object will belong to a certain type and many categories will be further divided into subtypes. Using one or more mask triples will allow you to filter the user selection for the type(s) of objects you are interested in. For example: does your journal only work on sheet bodies? You can set the mask triples so that the user can only select sheet bodies (not solid bodies, curves, datums, etc).

 

In addition to the GTAC examples, you might also look at:

http://nxjournaling.com/content/using-mask-triples-selectobject-routine

 

The article was written with NX 7.5 in mind; if you use NX 8 or newer, use the function .SelectTaggedObject or .SelectTaggedObjects instead of the deprecated .SelectObject or .SelectObjects.