Cancel
Showing results for 
Search instead for 
Did you mean: 

Set the Feature Collector to 0 C# NXOpen

Pioneer
Pioneer

Hi Guys,

 

Is there a Function to set the FeatureCollector back to 0 ?

For Example if the User select a wrong Feature i want to delete this selection of the Feature Collector. 

 

Thanks for every Answer !

1 REPLY

Re: Set the Feature Collector to 0 C# NXOpen

Phenom
Phenom

The SelectFeature block should have a method "SetSelectedObjects()". Just call this and pass in an empty array of TaggedObjects.

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Lenovo ThinkPad W540, Win7, 16GB. Developing in: Java | C | KF
Production: NX8.5.3.3 MP11 64bit Testing: NX9.0.2.5