Cancel
Showing results for 
Search instead for 
Did you mean: 

Settings or customer default that controls when .dll are loaded?

Creator
Creator

Is there a setting or customer default or some other method that changes when NX loads an internal .dll?

The reason I am asking is that for some reason, when I launch NX 11 using our companies custom profiles the first time I launch a command I need to wait 20+ seconds for the dialog to show up. However, if I do a clean launch without any of our customizations the dialog comes up in less than 4 seconds. Reviewing the log file for both shows that in the custom profile version NX is loading libuicom_modl.dll and libuicomp_mswp.dll right after clicking extrude, the clean launch log shows only libuicomp_mswp.dll being loaded and libuicom_modl.dll is loaded much earlier.

 

Custom profile launch

&MACRO MENU, 0, UG_MODELING_EXTRUDED_FEATURE UG_GATEWAY_MAIN_MENUBAR <rbn_modeling_home.rtb->rbn_feature.grb> ## ! 
UNDO_UG: Recyclable status of mark 11  set to False 
Successfully loaded dynamic module c:\appl\eng\ugs\nx11\nxbin\libuicomp_mswp.dll
Loaded module c:\appl\eng\ugs\nx11\nxbin\libuicomp_modl.dll 7fe9e1c0000 104000 34fb425a-4e3d1774-a82e8c-76a46377-1=libuicomp_modl___152345379064 version = 11.0.2.7
Loaded module c:\appl\eng\ugs\nx11\nxbin\libuicomp_mswp.dll 7fe9e2d0000 26000 47bd79ef-4aeb3ba4-6003d2ae-dc92cb1-1=libuicomp_mswp___152345285464 version = 11.0.2.7
Successfully loaded dynamic module c:\appl\eng\ugs\nx11\nxbin\libjaselectionintent.dll
Loaded module c:\appl\eng\ugs\nx11\nxbin\libjaselectionintent.dll 7fe9e120000 91000 e5b48df2-4f3d13bf-9fb69494-fa9bb2a7-1=libjaselectionintent___152345575864 version = 11.0.2.7

Standard launch

&MACRO MENU, 0, UG_MODELING_EXTRUDED_FEATURE UG_GATEWAY_MAIN_MENUBAR <rbn_modeling_home.rtb->rbn_feature.grb> ## ! 
UNDO_UG: Recyclable status of mark 14  set to False 
Successfully loaded dynamic module C:\appl\eng\ugs\nx11\NXBIN\libuicomp_mswp.dll
Loaded module c:\appl\eng\ugs\nx11\nxbin\libuicomp_mswp.dll 7fe96060000 26000 47bd79ef-4aeb3ba4-6003d2ae-dc92cb1-1=libuicomp_mswp___152345285464 version = 11.0.2.7
Successfully loaded dynamic module C:\appl\eng\ugs\nx11\NXBIN\libjaselectionintent.dll
Loaded module c:\appl\eng\ugs\nx11\nxbin\libjaselectionintent.dll 7fe95fc0000 91000 e5b48df2-4f3d13bf-9fb69494-fa9bb2a7-1=libjaselectionintent___152345575864 version = 11.0.2.7

Any advice on what could cause those .dll to be loaded at different times causing the delay I am seeing?