Cancel
Showing results for 
Search instead for 
Did you mean: 

Shifting point along CSYS axis

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello everyone!

 

How to obtain coordinates of a point shifted along axis of a given Datum CSYS? For example, of a point with coordinates 0,0,0 shifted along the Z-axis at a distance of 100. Obviously it would be 0,0,100 but what is the program method? Datum CSYS can be oriented at random angles so simply adding values won't work. I suspect that I should somehow use matrix transformation + csys methods, but I couldn't work it out. Can you please help?

2 REPLIES

Re: Shifting point along CSYS axis

Legend
Legend

A wrapper method exist for csys to csys.

 

Public Sub CsysToCsys (
from_origin As Double(),
from_x_axis As Double(),
from_y_axis As Double(),
to_origin As Double(),
to_x_axis As Double(),
to_y_axis As Double(),
mtx As Double())

 

Frank Swinkels

Re: Shifting point along CSYS axis

Creator
Creator

Hello,

I am not sure. To obtain the coordinates of DatumCsys, you can use features.Location property if the featuretype is DatumCsys. To edit/move the DatumCsys coordinates, use CreateXform method.

 

Thanks.