Cancel
Showing results for 
Search instead for 
Did you mean: 

Show Shortcuts - number of icons

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Just wondering if is possible change maximum number of displayed icons in dialogs, if options are displayed as shportcuts.

For example, in the dialog "Assembly Constraint" I swtich TYPE menu from LIST to SHOW SHORTCUTS. There are 6 icons. Is possible show shortcuts for all ten types of constraints?

 

Thanks for any help

 

2 REPLIES

Re: Show Shortcuts - number of icons

If you are referring to the UI, as far as I know theUI keeps the icons in a single row - 4 if there is a label for the option, and 6 if there is no label (as you see with Type).

 

If you are writing an API program, there are other UI blocks then enumeration that you may be able to use to display an array of icons.

Mark Rief
Retired Siemens

Re: Show Shortcuts - number of icons

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Many thanks for answer Mark