Cancel
Showing results for 
Search instead for 
Did you mean: 

Show blank CAM geometry NXOpen

Experimenter
Experimenter

Hi, 

 

I am wondering if it is possible to show the blank geometry with a NX open command. Show3DWorkpiece shows unfortunately only the workpiece after an operation, but not the initial blank. I could not find a similar function to show the blank (or part geometry). Within the NX user interface one can show the blank with the button shown in the picture.

picture_Workpiece_Blank.png

 

Does someone have an idea how to do this?

2 REPLIES

Re: Show blank CAM geometry NXOpen

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Have you tried recording a journal?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Show blank CAM geometry NXOpen

Experimenter
Experimenter
The Journal recorder doesn't record that action, unfortunately.