Cancel
Showing results for 
Search instead for 
Did you mean: 

Simple way to define creation of simple objects in specific layers

Builder
Builder

Hi,

We are looking for a simple way to define creation of simple objects in specific layers.

Like: Create Datum Planes only in Layer 10, or create lines and points in layer 20, etc.

 

Is there an easy way to define it?

 

Thanks a lot,

Idit Gvirtz

2 REPLIES

Re: Simple way to define creation of simple objects in specific layers

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

With few exceptions, objects are created on the current work layer. You will need to change the work layer before creating the object, or move the objects to the desired layers after creation. I know of no "out-of-the-box" method to automatically create/move a certain object type to a designated layer.

Re: Simple way to define creation of simple objects in specific layers

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The only 2 ways I can think of....

 

1) Before creation

Use Menuscript to add /PRE actions (to all object types you care about) to set the work layer "appropriately".  If you want to use ranges (e.g. all datums on layers 20-25) you could check the current layer is in that range, and if not, you'll have to figure out a rule as to which layer to use.

 

2) As a "cleanup" action

(possibly as a Manuscript "/PRE" action on all the "Save" options?) Examine all geometry, move to appropriate layer as needed.

 

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled