Cancel
Showing results for 
Search instead for 
Did you mean: 

Storing information in the NX assembly - UDO?

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

I have built an application that works well, but runs a long session that I would love to split into few separate ones. But that requires storing certain information from the previous session for use by the subsequent ones.

Do I understand it right that I can use UDO for that? Could you please advice?

5 REPLIES 5

Re: Storing information in the NX assembly - UDO?

Pioneer
Pioneer

Yes, UDO will help you alot in this aspect. I am using UDO too. Its too good to use to save info and use those in our programe. Those info will be saved in that prt file and your tool can retrieve as you feel like and modify the info too and can also use facility to link UDO to the Geometry.

Re: Storing information in the NX assembly - UDO?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The other options would be expressions or attributes.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Storing information in the NX assembly - UDO?

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
Indeed. But given the nature of data using attributes or expressions would be too cumbersome.

Re: Storing information in the NX assembly - UDO?

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Do you have a simple example of a data-storing UDO?

Highlighted

Re: Storing information in the NX assembly - UDO?

Siemens Phenom Siemens Phenom
Siemens Phenom

There is a UDO example delivered in the Sample Applications:

 

%UGII_BASE_DIR%\UGOPEN\SampleNXOpenApplications\<language>\UDO

 

where <language> is .NET, C++ or Java