Cancel
Showing results for 
Search instead for 
Did you mean: 

Suppress failed feature automatically when driving part externally.

Valued Contributor
Valued Contributor

Hello,

I have a part which imports expressions from .exp file. Sometimes combinations of the parameters result in the feature failure. It is usually expected Nx tree indicates the failed features. However sometimes read the .exp file and do nothing even the parameter combination is bad. This may cause confusion because you may think there is no problem with the parameters. I would like to know if there is an option which permits the bad features suppressed in the tree in any combination of the parameters?