08-03-2015 09:11 AM
Is there any way to keep the listing window from popping up when you run Certain methods.
For instance the UFClone.perfomClone automatically pops open the listing window. I would like to keep that from happening.
Please and thank you.
08-03-2015 09:24 AM
Lenovo ThinkPad W540, Win7, 16GB. Developing in: Java | C | KF
Production: [NX8.5.3.3 MP11 64bit] Testing: [NX12.0.0.27 MP1]
08-03-2015 09:58 AM
Until the developers change the function to suppress the listing window, you can use the listing window's .CloseWindow method. The user may notice a quick flash as the window is opened then immediately closed, but it may be better than leaving the window open.
08-03-2015 10:43 AM
You can try redirecting the output so that the list window does not appear in the first place. Use ListingWindow.SelectDevice() and set DeviceType to ListingWindow.DeviceType.None
08-03-2015 10:50 AM
I got a sense of deja vu from this thread, now I know why. Someone had the same question about 18 months ago:
According to the OP in the other thread, setting the listing window output to null did not have the desired effect.