Cancel
Showing results for 
Search instead for 
Did you mean: 

To code for "Execute" in NX 10.0

Pioneer
Pioneer

Hello,

Can I execute exe file using CTRL+U programmatically and browse .exe file in NX 7.5 and NX 10.0 using VB.net or C++ ?

Your help would be appreciable!

 

 

 

 

4 REPLIES

Re: To code for "Execute" in NX 10.0

Ken_A 1st Gear
1st Gear

Not really.

NX API code *to be run from an NX session* has to be a DLL.

You can have external API programs that run, but don't interact with a session.

You can "remote" into NX from a separate EXE, but NX has to be running - there are examples (search this forum for remoting)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
Apparently I've turned into a gearhead


Re: To code for "Execute" in NX 10.0

cowski1 3rd Gear
3rd Gear

In VB.net you can use the System.Diagnostics.Process.Start method. The journal below opens windows explorer. I'm sure there is a similar strategy for C++.

 

Option Strict Off
Imports System
Imports NXOpen

Module Module1

    Sub Main()

        Dim theSession As Session = Session.GetSession()
        If IsNothing(theSession.Parts.Work) Then
            'active part required
            Return
        End If

        Dim workPart As Part = theSession.Parts.Work
        Dim lw As ListingWindow = theSession.ListingWindow
        lw.Open()

        Dim myFolder As String
        ' change the "myFolder" variable to point to your folder of choice
        myFolder = My.Computer.FileSystem.SpecialDirectories.MyDocuments
        'myFolder = "C:\Temp"
        'myFolder = "C:\path\to\your\folder"

        Try

            System.Diagnostics.Process.Start("explorer.exe", myFolder)

        Catch ex As Exception
            MsgBox(ex.Message)

        Finally

        End Try

        lw.Close()

    End Sub


    Public Function GetUnloadOption(ByVal dummy As String) As Integer

        'Unloads the image when the NX session terminates
        GetUnloadOption = NXOpen.Session.LibraryUnloadOption.AtTermination

    End Function

End Module

 

Edit: After reading Ken's post, I realize that I may have misunderstood the question. The above code will open an .exe file from NX, but not one that interacts with the NX session.

Re: To code for "Execute" in NX 10.0

Siemens Phenom Siemens Phenom
Siemens Phenom

Ken's comment is correct if the program is written in C or C++.

 

But for programs written in NXOpen VB.Net or C#.Net, you can run an executable (.exe) using File -> Execute -> NX Open, within an interactive NX session, and it will run in the context of the interactive session, not as a separate forked process, just as if you were running a .DLL.

 

I know, weird, huh?  But that is how it works.  8-)

Re: To code for "Execute" in NX 10.0

Siemens Phenom Siemens Phenom
Siemens Phenom

> I know, weird, huh?  But that is how it works

 

It's because, in the .NET world, there is very little difference between a DLL file and an EXE file. In .NET jargon, both are these are considered to be an "assembly". Some further explanation here.

山田
yamada