Cancel
Showing results for 
Search instead for 
Did you mean: 

To create an Exe application in C++ using NX wizard 7.5

Pioneer
Pioneer

Hello,

Im new to NX programming. Can you please help me with :

How to create an exe application in C++ using NX wizard 7.5 and to get  NX session ?

Also wanted to confirm that is it same using NX wizard 10.0?

 

 

Regards,

Juhi

2 REPLIES

Re: To create an Exe application in C++ using NX wizard 7.5

Ken_A 1st Gear
1st Gear

NX7.5 and NX10 require different versions of Visual Studio / C++

In addition, the NX wizards are different.

NX7.5 requires VC++ 2008 (I think SP1?)

NX10 requires VC++ 2012 update 1

 

In general, if you have an application developed for NX version "X", and you need to upgrade it to support NX version "Y", Siemens recommends creating a NEW project in the new VC++ with the new (version "Y") NX wizard, and then copying the required files/code over.

 

Hope this helps...Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
Apparently I've turned into a gearhead


Re: To create an Exe application in C++ using NX wizard 7.5

Pioneer
Pioneer

Thanks for your valuable help. It worked!

I want to know what code should i write to get the NX session, to open it, get the part, display part, get assembly and display it  using C++? For NX 10.0 and NX 7.5 versions.

 

 

Regards,

Juhi