cancel
Showing results for 
Search instead for 
Did you mean: 

Tool Path - "missing" motions?

Siemens Creator Siemens Creator
Siemens Creator

Hi,

I’m trying to do the following:

Take a PRT file that contains Point to Point operations, run Find Features option (STEPs features only) and tells which Point to Point operation process each feature.

 In order to do so I need to get all the motions from the operations tool path.
Unfortunately, on a significant part of operations, some motions are “missing”.
(Assumption: Maybe they appear as “SYSTEM” motions instead of "LINEAR" motions?)

The assumption above is based on the following:

cover.jpg
(Sourcehttps://community.plm.automation.siemens.com/t5/NX-Programming-Customization/Change-direction-points...)

 

Is this related to my case? If so, is there a way to overcome this issue?
If not – what did I miss?

 

Thanks,

Tal.