Cancel
Showing results for 
Search instead for 
Did you mean: 

UGS license bundle

Pioneer
Pioneer

Hi,guys

Do you meet this problem as attached image. NX let me setup this buddle every time at openning of NX.

 

 

UGS LICENSE BUNDLE.PNGUGS LICENSE BUNDLE2.PNG

-----------------------------------------
UG3.0
UG6.0
NX10.0.35
NX11.0.1
UG_NX is my favorite !!!!!!
5 REPLIES

Re: UGS license bundle

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You don't state what version you are using.

1) You can define UGS_LICENSE_BUNDLE to point to TOTALMACH

2) You can use the Siemens licensing tool to set the bundle

 

Be aware at some point the licensing tool was changed to use the registry, and from that verison of NX onwards, the registry value over-rides the ENV variable

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: UGS license bundle

Legend
Legend

add following line to startup script

 

set UGS_LICENSE_BUNDLE=TOTALMACH

 

or add system/user environment variable to the pc

 

Frederik Verscheure
Evolve Consulting bvba
Freelance NX & Teamcenter consultant
frederik@evolve-consulting.be

Re: UGS license bundle

Experimenter
Experimenter

How should the environment variable be declared?

Re: UGS license bundle

Pioneer
Pioneer

Yes

-----------------------------------------
UG3.0
UG6.0
NX10.0.35
NX11.0.1
UG_NX is my favorite !!!!!!

Re: UGS license bundle

Legend
Legend

 

open commandline:

type following line

 

setx UGS_LICENSE_BUNDLE TOTALMACH

 

screenshot_000202.jpg

Frederik Verscheure
Evolve Consulting bvba
Freelance NX & Teamcenter consultant
frederik@evolve-consulting.be