Cancel
Showing results for 
Search instead for 
Did you mean: 

UGZip

Legend
Legend

Has anyone considered updating or modifying the UGzip program to use 7zip compression?

I use it regularly for archiving.

 

Such a thing is well beyond my abilities, but maybe one of you could?

 

http://7-zip.org/

7-Zip is open source software. Most of the source code is under the GNU LGPL license. The unRAR code is under a mixed license: GNU LGPL + unRAR restrictions. Check license information here: 7-Zip license.

You can use 7-Zip on any computer, including a computer in a commercial organization. You don't need to register or pay for 7-Zip.
Rob Newcomb, Design and Engineering manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r8 /WorkNC 2020.0
Testing:NX 1855
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro
7 REPLIES 7

Re: UGZip

You would need to contact the author of the program, or whoever is maintaining the source code. A long time ago is was Weidemann engineering, but I don't know the current status.

Mark Rief
Retired Siemens

Re: UGZip

Legend
Legend

Hi,

 

 

 

Where can i find this UGzip?

 

br

Fred

Frederik Verscheure
Evolve Consulting bvba
Freelance NX & Teamcenter consultant
frederik@evolve-consulting.be

Re: UGZip

Legend
Legend

http://www.w-eng.de/

Rob Newcomb, Design and Engineering manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r8 /WorkNC 2020.0
Testing:NX 1855
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro

Re: UGZip

Legend
Legend

GTAC has a replacement tool for this UGZip

https://solutions.industrysoftware.automation.siemens.com/view.php?sort=desc&q=.net+license&dt=nx-ap...

 

Frederik Verscheure
Evolve Consulting bvba
Freelance NX & Teamcenter consultant
frederik@evolve-consulting.be

Re: UGZip

Legend
Legend

while this does use 7zip. its commandline based.

 

if you just run the journal, it'll 7zip every open file and stick it in your temp.

 

I havent tried to run it per the instructions yet.

 

 

 

Rob Newcomb, Design and Engineering manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r8 /WorkNC 2020.0
Testing:NX 1855
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro

Re: UGZip

Legend
Legend

yes, the zip-package goes to your %UGII_TMP_DIR%.

 

Attached a updated journal that asks the output folder and it will store the last output location in the windows registry.

Just edit the location where 7zip is installed (line 97-102)

Frederik Verscheure
Evolve Consulting bvba
Freelance NX & Teamcenter consultant
frederik@evolve-consulting.be

Re: UGZip

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

The script that @evolve provided works great.

I modified it to have some extra features.

  1. Added a Regular Expression match to find a master model draft by name.
    So if you make your drawing by appending a suffix like _dwg.prt then it will find it if it is in the same folder.
    In the following image you see [BASENAME], that is replaced with the file name by the script.
    The \d matches a single digit. You can find RegEx testers on line to help you craft your match.
  2. Added an argument to force gathering all the session parts.
    I found that it was including my machining templates if they were loaded.
  3. Added an argument that is a |"pipe" separated list of paths to exclude if the file resides there.
  4. Made a YouTube of the installation process.
    https://www.youtube.com/watch?v=kQWfbCcGpI
    The file is attached as text.

PackAndGo.PNG

LMGi
www.TLMGi.com