Cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to map unit definition g/cm^3 for parameter MassDensity

Legend
Legend

NX 10.0.3.5

 

I try to assign Material from Classification library where in MatML dataset defined units for Density in

g/cm^3

 

And as result I've got that error - Unable to map unit definition g/cm^3 for parameter MassPropsDensity.

 

I also found that units in kg/m^3 works fine, but if I change units to g/cm^3 - this error occure.

 

I saw one PR on GTAC site with similar problem -PR #:7732439

 Unable to map unit definition mm^2/N(1/MPa) for parameter Volumetric Deformation Constants

 

 But there is no workaround for that PR, only recommendation to try this in NX11

 

Does workaround for this subject exist?

2 REPLIES

Re: Unable to map unit definition g/cm^3 for parameter MassDensity

Legend
Legend

it was non english localization issue. I just created MatML from NX in english locale and problem was solved.

Re: Unable to map unit definition g/cm^3 for parameter MassDensity

Innovator
Innovator

@alex_c wrote:

it was non english localization issue. I just created MatML from NX in english locale and problem was solved.


I am having a similiar issue, but with Poisson's ratio and Thermal Coefficient Expansion.

This was not an issue prior to NX 11.0.1.

 

How does one create a MatML (XML) from an english locale? I am running a German version of Windows 10.

 

Thanks!

Marc Prosl
NX Software Developer