Cancel
Showing results for 
Search instead for 
Did you mean: 

Update the size (height) of a Listbox (UI builder)

Gears Phenom Gears Phenom
Gears Phenom

To all

 

I am making some "cosmetic" changes/adjustments to a code containing a UI Builder GUI with Listboxes. I'd like to change the "height" of a list box depending on the count of the list going into that listbox. Does anyoone know in which functions one should put the following lines?

 

Thanks

Regards

 

If myList.Count < 10 Then
	myLboxInGUI.Height = myList.Count
Else
	myLboxInGUI.Height = 10
End if	

 

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)
4 REPLIES

Re: Update the size (height) of a Listbox (UI builder)

Phenom
Phenom

Some things, including setting the height of a ListBox, can only be done when designing the dialog or in the initialize() method.

So you need to set the height of your ListBoxes in your initialize() method.

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Lenovo ThinkPad W540, Win7, 16GB. Developing in: Java | C | KF
Production: [NX8.5.3.3 MP11 64bit] Testing: [NX12.0.0.27 MP1]

Re: Update the size (height) of a Listbox (UI builder)

Gears Phenom Gears Phenom
Gears Phenom

Thanks Graham for confirming rhis. Bit of shame as I would have liked to update the "height" every time a list is created and dispalyed.

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)

Re: Update the size (height) of a Listbox (UI builder)

Siemens Phenom Siemens Phenom
Siemens Phenom

For future reference, this could also be confirmed via the online documentation. The online documentation for each block contains a table with an "Access" column that details where each property can be modified or read:

 

https://docs.plm.automation.siemens.com/tdoc/nx/10/nx_api/#uid:index_blockstyler:id1153911:id1154006...

 

The List Box height property is listed as CIG, which means that it can be set at Creation (in the Block UI Styler) or in the Initialize callback. It does not contain an S in the access column, which would mean that it could be Set in any callback.

Re: Update the size (height) of a Listbox (UI builder)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you want to update the size during execution, you'll probably have to file an ER.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled