Cancel
Showing results for 
Search instead for 
Did you mean: 

Updating from NX9 to NX11custom

Phenom
Phenom

Upgrading from NX9 to NX11, along with Tc9 to Tc11, so while everyone is offline for the Tc upgrade, I want to migrate the user files from the NX9custom to NX11custom location.

 

Do all the files need to go, or only certain ones?

These I am bringing for sure:

role folder

history_ugmgr.pax

DialogMemory.dlx

user.mtx

 

Anything else, that will make the move as seamless as possible for users, and keep my phone from blowing up after the upgrade?

 

Or would you suggest I migrate everything, and let NX11 update/change whatever it needs?

-Dave
NX 11 | Teamcenter 11 | Windows 8.1
1 REPLY

Re: Updating from NX9 to NX11custom

Esteemed Contributor
Esteemed Contributor

I would think about not doing most of them.

I realize the user ends up more "as installed" GUI, but some things (e.g. dialog memory) may hide stuff that's new in NX11.

 

Note also, NX11 will FORCE the "ribbon" GUI.  If anyone was still using the legacy "toolbars" interface, I'm not sure how the old files will help (and they might hurt)

 

I don't migrate anything for our users (but then I might not hear the wailing & gnashing of teeth when they open the new version ;-).  Some users will try reloading roles or whatever, but I leave that up to them.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled