Cancel
Showing results for 
Search instead for 
Did you mean: 

Urgent help needed -CAM customization (drilling operation )

Pioneer
Pioneer

Hi All,

 

The requirement is that I have to change the minimum clearance value in the selected drill operation.

 

I am running a machine simulation(only for drilling operations )using NX open dll.

  1. while running the simulation, if there is violation of clearance values then I have to check for th cycle event->minimum clearance value for a selected drill operation.
  2. I have to change it to next value and then run the simulation again.
  3. I have do this till i will get a error free simulation.

Now for this, I am trying to change my cycle event->minimum clearance value in drill operation but I am unable to achieve it.Can anyone please help me with the solution.

 

Regards

img@work

2 REPLIES

Re: Urgent help needed -CAM customization (drilling operation )

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Point-to-point (legacy) drill operation?

or (new) holemaking operation?

Or both?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Urgent help needed -CAM customization (drilling operation )

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Would be nice to not cross-post, since the answers are already in another thread in this forum.

Might be best to lock this thread as a duplicate.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide