Cancel
Showing results for 
Search instead for 
Did you mean: 

Use the NX interface (UI block styler) outside of NX

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello,

 

Is it possible to use the UI block styler outside of NX? In my own application I would like to use the interface of NX, is it this possible?

 

Thanks,

 

Best regards,

 

 

 

 

3 REPLIES 3

Re: Use the NX interface (UI block styler) outside of NX

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The block dialogs are only supported inside of an interactive NX session as far as I know.

If you need dialogs without an interactive NX session, you need to use regular WinForm dialogs.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Use the NX interface (UI block styler) outside of NX

Solution Partner Genius Solution Partner Genius
Solution Partner Genius
Thanks Stefan Smiley Happy

Re: Use the NX interface (UI block styler) outside of NX

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Furthermore, UI need an open work part. You cant lauch a UI block styler dialog from the gateway. If you need so, your code should create a dummy part, then open the UI and when finished, close the part. It will be trasnsparent to the user.

 

Elias.