Cancel
Showing results for 
Search instead for 
Did you mean: 

User Defined Feature (UDF) vs UDO

What is the difference between a User Defined Feature (UDF) and udo

3 REPLIES 3

Re: User Defined Feature (UDF) vs UDO

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

A UDF requires no knowledge of API code, so can be done by anyone (note there may be some setup required for NX to find the UDFs you define)

 

A UDO (patricularly a UDO "feature") requires API programming, but can have a richer range of behaviors.

 

Note NX 11 introduces a new (API only) way of defining custom features as well (but all I know about it is that it has been mentioned here in the community site)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: User Defined Feature (UDF) vs UDO

Thank you.

 

But i have one query. Is "UDO feature" and "custom features of NX 11" same??

Re: User Defined Feature (UDF) vs UDO

Siemens Genius Siemens Genius
Siemens Genius

No they are not same.

SE-Advanced
Siemens Industry Software