Cancel
Showing results for 
Search instead for 
Did you mean: 

Using NXRemotable objects

Innovator
Innovator

Since Tagged object derives from NXRemotable which derives from MarshRefObj, that means we shuld be able to use marshalling services for the object sin a given session, transfer them over a server and then use them. But I can't seem to get it to work. Has anybody dealt with stuff like this?

 

In the log file, when you load up a session of nx, it opens and establishes a port for interoperations. 

Is there any documenation or help? Thank you.

1 REPLY 1

Re: Using NXRemotable objects

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

see

%UGII_BASE_DIR%\UGOPEN\SampleNXOpenApplications\.NET\RemotingExample

for an example of remoting

you can replace ".net" with "Java" if you would prefer Java instead of C#

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled