Cancel
Showing results for 
Search instead for 
Did you mean: 

Using SelectionManager.SelectTaggedObject

Innovator
Innovator

How do you get a component from the tag using the user has selected from 

theUI.SelectionManager.SelectTaggedObject("Select a curve", "", Selection.SelectionScope.AnyInAssembly, false, curveType, out type, out cursor);

2 REPLIES

Re: Using SelectionManager.SelectTaggedObject

Siemens Phenom Siemens Phenom
Siemens Phenom

 

The Curve class has a property called "OwningComponent" that should allow you to determine what component the selected curve belongs to.

 

Re: Using SelectionManager.SelectTaggedObject

Honored Contributor
Honored Contributor

The .SelectTaggedObject method returns a TaggedObject, not a tag (though you can get the tag from the TaggedObject if needed). You may need to cast the TaggedObject to a Curve object before accessing the .OwningComponent property as suggested by Steve.