Cancel
Showing results for 
Search instead for 
Did you mean: 

Using UGII_BACKGROUND_URL

Honored Contributor
Honored Contributor

I want to use UGII_BACKGROUND_URL to use a custom background when NX starts, or no parts are loaded.  I know I did this in the past and had the image auto size to fit the NX window, but that was 2 employers ago, and the html brain cells are really dusty.

 

Google searches keep pointing me to use a style sheet, but I thought I did it all html, any thoughts on this?  I want it simple.

 

Right now my code is shown below, but I get scroll bars:

<html>

<img src="background.jpg" style="border: none; height: 100%" />
	
</html>
-Dave
NX 11 | Teamcenter 11 | Windows 10
1 REPLY 1

Re: Using UGII_BACKGROUND_URL

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The header for my .html file:

<HTML>

<HEAD>
   <TITLE>NX10 Upgrade Issues</TITLE>

   <LINK rel="stylesheet" href=".\post_docs.css" type="text/css"> 
</HEAD>
<BODY>
<!-- Stuff here -->
</BODY>
</HTML>

 the CSS (partial):

 

/*
 * Style sheet for system build/software installation on-line documentation
 * v1.0	KG Akerboom		01-Sep-2001		Initial version
 */

/* Overall items */
	H1 { font-weight: bold; text-align: center	 } 
	H2 { font-weight: bold;			} 
	H3 { font-weight: lighter;		} 
	H4 { text-indent: 2em			}
	DT { font-weight: bold;			}

/* other stuff omitted */
Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled