Cancel
Showing results for 
Search instead for 
Did you mean: 

View Creation problem in drafting

Builder
Builder

Hello Everyone 

I have a part and I would to create it 1)front view, 2)Side view  3)Top view and 4)  Isometric view in drafting with help of coding.

There are 2 ways to create that views

1) View Creation Wizard

2) Base View Command

Which way would be better out of the two?

Part1.PNG

Is any code snippest or journal or examples?

2 REPLIES 2

Re: View Creation problem in drafting

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Krishna11 ,

In my opinion 'View creation wizard' command would be better. In journal, less lines of code would be there in case of 'View creation wizard' as compared to 'Base view command'.

Thanks,

Amol

Re: View Creation problem in drafting

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Please note that you can set up your drawing template with various views pre-defined in the template. When you create a new drawing of a part, the views of the part will be created automatically in the template (no code required!). This might be a faster and easier way to get what you want.