Cancel
Showing results for 
Search instead for 
Did you mean: 

Where are the NX JT export setting stored ? (except than PVTRANS\tessUG.config)

Valued Contributor
Valued Contributor

Hi nice people of NX,

 

Here are the steps regarding my question :

- Open NX (using NX9 but seems to be the same with NX10 and 11)

- Open a part

- Export -> JT

- In the tesselation tab, add LOD to have 4 levels (or any other modification of the number of level)

- Export JT

- Close NX

- Open NX

- Open the JT export window, see that there are 4 LOD but PVTRANS\tessUG.config nor pvtrans\ot_pub\application\tessOTPub.config contain that number of LODS or any modifications I can see in the NX export JT window settings UI.

 

TLDR : Where are the LOD settings (for NX UI) saved/serialized ?

 

Thanks guys.

 

 

1 REPLY

Re: Where are the NX JT export setting stored ? (except than PVTRANS\tessUG.config)

Valued Contributor
Valued Contributor

Related issue/question: in NX9 API, is there a trick so that calling JtCreator:Smiley FrustratedetConfigFile makes that the LOD setting of the JtCreator are set ?

If not, is there a function/method to read a .config file ?

 

I feel I'm missing something here...