Cancel
Showing results for 
Search instead for 
Did you mean: 

Why doesn't this work?

Innovator
Innovator

Here is my code

///////////////////////

using System;
using System.Collections;
using System.IO;
using Microsoft.VisualStudio.TestTools.UnitTesting;

namespace Test
{
[TestClass]
public class UnitTest1
{

[TestMethod]
public void TestMethod1()
{
System.Environment.SetEnvironmentVariable("SESSIONNAME", "Console");
System.Environment.SetEnvironmentVariable("UGII_UGOPENPP", @"C:\Program Files\Siemens\NX 9.0\ugopenpp");
System.Environment.SetEnvironmentVariable("UGII_USERFCN", @"C:\Program Files\Siemens\NX 9.0\ugopen");
System.Environment.SetEnvironmentVariable("UGII_LANG", "english");
System.Environment.SetEnvironmentVariable("UGII_JAVA_HOME", @"C:\Program Files\Java\jre1.8.0_25");
System.Environment.SetEnvironmentVariable("SPLM_LICENSE_SERVER", "28000@CTS-SERVER");
System.Environment.SetEnvironmentVariable("UGII_LICENSE_FILE", "27000@CTS-SERVER");
System.Environment.SetEnvironmentVariable("UGII_ENV_FILE", @"U:\NX90\Concept\NX90custom\NX90library\NX90env.dat");
System.Environment.SetEnvironmentVariable("UGII_BASE_DIR", @"C:\Program Files\Siemens\NX 9.0");
System.Environment.SetEnvironmentVariable("NX_NUMBER", "NX90");
System.Environment.SetEnvironmentVariable("UGII_ROUTING_KIT_UNITS", "metric");
System.Environment.SetEnvironmentVariable("UGII_ROUTE_UGMANAGER_MODE", "FALSE");
System.Environment.SetEnvironmentVariable("NX_CUSTOM_DIR", @"U:\NX90\Concept\NX90custom");
System.Environment.SetEnvironmentVariable("NX_CUSTOM_LIB", @"U:\NX90\Concept\NX90custom\NX90library");
System.Environment.SetEnvironmentVariable("NX_PACKAGE_NAME", "NX");
System.Environment.SetEnvironmentVariable("UGII_ROOT_DIR", @"C:\Program Files\Siemens\NX 9.0\ugii\");

NXOpen.Session ses = NXOpen.Session.GetSession();
NXOpen.PartLoadStatus status;
ses.Parts.OpenDisplay(@"G:\0Components\fasteners\metric\shcs\020\20mm-shcs-065.prt", out status);

}
}
}

//////////////////////////////////////

 

My question is why does this raise a System.BadImageFormatException when I runt the test with the actual Microsoft.VisualStudio.TestTools.UnitTesting framework?

Are all my enviornment variables being set correctly? Am I missing one?

Is there something else I need to do?

 

 

2 REPLIES 2
Highlighted

Re: Why doesn't this work?

Siemens Phenom Siemens Phenom
Siemens Phenom

BadImageFormatException can mean that you built an image for Win32 or AnyCPU, instead of x64, or it might mean that you are trying to use the wrong version of the .Net Framework.

 

And a side note - we do not recommend setting environment variables within an NXOpen program.  We always suggest that you set them outside of the program first.  If you run your program from an NX Command Prompt, then they should all be set correctly for you.  If you are running inside the Visual Studio, then you should start the studio session from an NX Command Prompt, to inherit all the right settings.

 

Re: Why doesn't this work?

Creator
Creator

Hi,

Follow the following process to resolve the issue.

1) Open the Test project from NX command shell.

2) Select Test->Test Settings->Default Processor architecture->x64

 

Now run the test. It will be success.